Configure the AKD Drive

The Configuration tab under the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costsAKD tab allows you to configure drives once the following conditions have been met:

  • The scan has been performed
  • Your project is compliant with the physical devices on the EtherCAT network
  • You have activated the Online Configuration mode

You then have access to all of the AKD configurations and parameters.

  1. In the Project Explorer, double-click the new AKD Drive or select Configuration from the context menu to open all the parameters linked to it.
    AKD Configuration
  2. Figure 5-31: AKD Configuration

  3. Define the motion parameters in the Limits tab to configure the limited motor torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist, speed, and acceleration

  4. Define the motion parameters in the Position Loop tab to configure the limiting following error.

  5. Define the resolution of the feedback position in the Feedback tab
    Note that for all feedback types, the motor position feedback sent from the AKD drive to the controller through EtherCAT is normalized to 20 bits/rev or 1048576 counts/rev
  6. Then, you must define the units to be used for the motion 1The normal units screen in the AKD Work bench GUI is not included in the IDE :
  7. To ensure high performance, define the load for your servo system.. KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger provides several options for performing the drive tuning:

For more details on AKD configuration, AKD Drive

For more details on AKD Firmware Download, refer to the FAQ section.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen